Part Number: TPA3116D2 Tool/software: Hello,
I'm building an amplifier based on TPA3116D2 in PBTL mono configuration.
I would like to drive a 6ohm sub-woofer, rated 120W.
I'm going to use a 24V supply.
From figure 22 and 26 of datasheet I can only…
Part Number: TPA3116D2 Tool/software: I am facing to pass the BCI tests while using this amplifier board. Noise getting between 20 mhz to 200 mhz.
Can you please someone guide to me how to resolve this issue
Part Number: TPA3116D2 Tool/software: Hello, use tpa3116d2 to design the power amplifier, the load is 4ohm, the power supply is 24V, and the output L = 33uh, C = 0.68uf. PWM = 400khz. SDZ and MUTE controlled via dsp.
Power-on sequence: 24V on--- > SDZ_HIGH…
Hi Jesse,
We use the TPA3116D2 but we can't use the PBTL mode(BTL mode is normal), can you also review the schematic again and check if there are any error for this design, thanks.
Part Number: TPA3118D2 Other Parts Discussed in Thread: TPA3116D2 , Tool/software: Hello, I would like to use an existing amplifier board design built around two TPA3118D2 amplifiers (to provide 4x30W 8 Ohm output). But as far as my research on this forum…
Part Number: TPA3116D2 Hello, I am new to this forum
I see this has been a problem by the posts on the net, As with the others, when a signal is high the audio cuts and then resumes,
there is nothing wrong with the heat sinking, nor the 0 volt connections…
Part Number: TPA3116D2 Hi,
I'm working on the TPA3116 amplifier. Config : Gain = 26dB, PVcc = 24V, RL = 2 Ohms, in PBTL mode.
- I'm able to have +90W but with THD = 7-9%. Is it normal to have that much THD to obtain near 100W ?
- Is the initial…
Part Number: TPA3116D2 Dear TI experts,
My customer considers TPA3116D2 for their new project, and they have a question about BD/1SPW modulation.
BD modulation is described as follows in the datasheet;
- This is a modulation scheme that allows operation…