Part Number: TPA3116D2-Q1 Other Parts Discussed in Thread: TLV320AIC3109-Q1 Hi team,
My customer want to use our audio device.
And the requirements are as below:
1.Analog Speaker amps: Automotive; Power supply is 3.3V or 5V; Output power needed is 28W;…
Part Number: TPA3116D2-Q1 SCH_Caravan_SPDIF_Rev3__20220329.pdf
Dear TI,
I use powerIC to design the circuit,there is one issue need your support.
due to the powerIC fully controlled by hardware, there is a big pop(about 500uV) happen when the power supply…
Part Number: TPA3116D2 Since the TPA3116D2DAD currently has no availability, I need to find to replacement and prefer a drop-in replacement, if at all possible. It appears that the TPA3116D2-Q1 (automotive) part is the most likely candidate, but there…
Part Number: TPA3116D2-Q1 Hello, thanks for taking the time for helping me with this doubt.
I want to design an audio power amplifier using the TPA3116D2-Q1. I had read the datasheet but is not clear to me the design procedure explained there. How should…
Part Number: TPA3116D2-Q1 Hi team,
Does TPA3116D2-Q1 have control sequence requirements for SDZ and MUTE pins during power on and power off? If yes, what is the control time interval between SDZ and MUTE
Part Number: TPA3116D2-Q1 Hi, Support Team
Currently during a PR event, 48 units were produced, but two units have different AUDIO LEVEL measurements.
Circuit condition: P-LIMIT MAX, 36dB GAIN
Operating conditions: 1KHz SINE WAVE PLAY, AMP input level…
Part Number: TPA3116D2-Q1 Other Parts Discussed in Thread: TPA3116D2 Hi Team,
I'd like to request the layout review of TPA3116D2-Q1. Please refer to the layout and schematic file below, check it and let me know the review result.
TPA3116D2-Q1_Layout…
Part Number: TPA3116D2-Q1 Other Parts Discussed in Thread: TAS6421-Q1 i require a high temperature class-d amplifier: Now the TPA3116D2-Q1 does state operation to 125'C, that is good.
My circuit needs to operate for 16 seconds at temperaures between…
Part Number: TPA3116D2-Q1 Other Parts Discussed in Thread: TPA3126D2 , TPA3116D2 Please delete this post if it is not appropriate however I wanted some help with choosing the correct power amplifier.
The requirements were as follows:
Up to 50W per channel…
Hello Jeff,
thank you for your advice.
I want to trying to drive 1 channel with impedance about 0.5 ohm.
I saw TAS6424, but I want an analog inputs. TPA3116D2-Q1 is cheaper, less complicated etc. When I use a PBTL mode with TPA3116D2-Q1, theoretically I…