Part Number: TPA3129D2EVM Tool/software: Thanks for response. I have few questions:
Switching frequency according to table 6 may be 400, 500, or 600 kHz. According data sheet it may be I watched 5.4 Mhz. What is right?
Describe please these :" In…
Part Number: TPA3129D2EVM Tool/software: I checked TPA3129 evaluation board. We need to use it in sync mode. I have changed R7=100k and R5=16, as result voltage on GVDD=5.9V and GAI/SLAVE=5.07V. In this case amplifier must come to slave mode, when switching…
Hi Michael,
I will address your questions below:
1. TTL logic refers to transistor-transistor logic levels, where typically a 5V supply is used. 2V to 5V would be considered a high, and 0 to 0.8V would be considered low.
In this case the SDZ can…