Hi Tapas,
I haven't heard back from you I'm assuming you were able to resolve your issue. If not, you just post a reply or create a new thread if this thread has locked due to time-out.
Best Regards
José Luis Figueroa
Audio Applications Engin
Part Number: TPA6203A1 I am using the Device as per the data sheet. However we are getting the device over heating and failing. I do have a "heatsink via the base of the device soldered onto the pcb tracking, but not to anything else.It looks like thermal…
Part Number: TPA6203A1 Other Parts Discussed in Thread: TPA6201A1 , , TPA6205A1 Hi,
Could you provide the thermal resistance of junction to package top of DGN?
I would like to know that of TPA6201A1. Datasheet shows only Theta-ja which is converted…
Part Number: TPA6203A1 Hi,
I am working with TPA6203A1 mono amplifier. I need to design a noise-free amplifier.
I saw 85-db PSRR for 90hz to 5khz from datasheet. I have calulated ripple value from that. Check check whether my calculation is correct…
Part Number: TPA6203A1 Hello,
Can we connect the output of TPA6203A1 to other output of D class amp? Please see the attached image. When we use D class amp, the TPA6203A1 in shutdown mode. Since the input impedance is high and output impedance will…
Doc1.pdf
Hello
Thanks for quick response.
Attached is the schematic of the circuit that I am testing. As I mentioned in my post, this is just the fully differential amplifier implementation of the recommended circuit for 8Ohm load. The AC characteristics…
Hi Tachibana-san,
In fact, It is possible to use TPA6203A1 with single-ended output, but you must consider adding a coupling capacitor as it is required to block the DC offset voltage from reaching the load. You could refer Differential Output Versus…
Part Number: TPA6203A1 Hello
Our customer want to know DISSIPATION RATINGS of DGN(MSOP) Package.
(Other package's one is described in the current data sheet.)
Please show this.
Regards,
Hajime Akahori
Part Number: TPA6203A1 The TPA6203A1 does not specify capacitive load drive capability or provide a plot for small-signal overshoot vs. capacitive load. Is this not an issue with this device due to internal compensation technique?
Part Number: TPA6203A1 Hi,
My customer is confirming the stability of TPA6203A1. He's eager to know method for measurement of Open Loop Gain/Phase.
<Question> Regarding Datasheet Page.8 Figure 24.(OPEN LOOP GAIN/PHASE vs FREQUENCY)
Is this the result…