Part Number: TPA6404-Q1 Hi Team,
My customer now use TPA6404.
During the test, when power off, there are some POP noise occurred. It came out after stadby and mute pulled down 720us
Customer want to confirm whether POP noise could be muted after standby…
Part Number: TPA6404-Q1 Hi Team,
Here are two questions may need your kindly help.
Bit[2]
Which DC diagnostic fault refers to in bit [2] in register 0x09, such as S2G, S2P, OL, SL?
Verification step
1: 4 CHs are connected to 4ohm load respectively …
Part Number: TPA6404-Q1 When using in 24V system, if the 24V battery connect to OUTP and OUTM pin accidentally. Does TPA6404 have protection to avoid damaging the TPA6404?
Besides the above question, do we have more detailed internal block diagram? Customer…
Part Number: TPA6404-Q1 Hi TI expert,
I am using TPA6404 in a automotive infotainment product, this speaker PA in integrated in a head unit PAD, the PCB area is very restricted and height is small.
My question is, I see that TPA6404 is a closed loop class…
Part Number: TPA6404-Q1 Tool/software: Code Composer Studio Hi,
I also would like to get the full datasheet of TPA6404-Q1 .
Could you send it to li.nan@dayin-tec.com?
Best Regards,
Li nan
Part Number: TPA6404-Q1 At the position after the CODEC we measure 10µV if the TPA6404 is disconnected. When we connect the TPA6404 the noise increses to 35µV at the same position (after the CODEC, on the inputs of the TPA6404). As a result…
Part Number: TPA6404-Q1
Hi,
I also would like to get the full datasheet of TPA6404-Q1.
Could you send it to kuramochi@fujiele.co.jp?
Best Regards,
Kuramochi
Part Number: TPA6404-Q1 Hi TI guys:
I'm evaluating TPA6404-Q1 on my new project, but i can't find the full datasheet on WWW.TI.COM, could you share me the full datasheet, thx
my E-mail is: jack.deng@wtmec.com
Part Number: TPA6404-Q1 Hi,
Recently we had a issue in FM sensitivity i.e. Tuner not able to pick-up signal and produce audio at low signal strength condition. Especially at the Frequency 90.8 MHz FM Station.
Based on our analysis, we found that 2.1…