Part Number: TPIC44H01
Hi Team, seeking some clarification.
Checking the TPIC44H01 datasheet and noticed that the OVLO would set it at a minimum of 27.5V but the VPWR should survive up to 40V.
First we want to know if this feature can be disabled…
Part Number: TPIC44H01 Hi,
I am currently looking for a Quad (or Octal) high side driver that can support line voltage up to 32V.
I have checked the TPIC44H01 datasheet and noticed that the OVLO would set it at a minimum of 27.5V but the VPWR should…
Other Parts Discussed in Thread: TPIC44H01 I have a customer who wants to use the TPIC44H01 high side driver to PWM an external MOSFETs at 15kHz. However, the gate driver current of the TPIC44H01 is only +/- 2mA so, they are considering adding a boost…
Other Parts Discussed in Thread: TPIC44H01 I have an application where the FET driver power is supplied with 24VDC and logic Vcc is supplied with 5VDC. The 24VDC is supplied through a separate connecter from the logic interface.
Power Connector: GND…
Other Parts Discussed in Thread: TPIC44H01
I'd like to know the frequency range of load switching using parallel control on TPIC44H01.
I need to control a
solenoid (high-side driver) through a PWM with Duty Cycle ranging from 0 to 100% with an…
Hi, Adrian,
This device is closer to the IFX part, but requires external FETs: tpic44h01
I am going to ask our colleagues in PSIL to comment if they have a similar device.
Hi Eggsy,
We have a low speed 4mA drive 4 channel highside gate driver, TPIC44h01, which can drive the inputs in parallel or serial with SPI.
Each channel is equipped with protection features.
This device is low speed and used for always ON/OFF 100…
Hi Umamahesh,
Great to hear from you!
We don't have an exact replacement for the MIC5013, but we has some that might work for your customer.
We could use one of our standard drivers like tpic44h01 and maybe add some external circuitry, especially…