Part Number: TPS1211-Q1 Hi Expert,
May I check two questions regarding to TPS1211?
Does the output reverse polarity protection work when the part is configed as driving one external MOSFET as the figure below?
2. Does the part remain turn…
Part Number: TPS1211-Q1 Hi sir,
Could you pls kindly suggest?
Can TPS12111 work normally with out Pre-charge condition?
If no use pre-charge, how to connect Pin G & INP_G?
Thanks a lot!
Part Number: TPS1211-Q1 Dear all
The schematic would operate in 125℃.
In order to meet this requirement, I need to calculate pulse width and pulse power of the resistors that R10, R6 and R41. Then I could define the specific part number of the resistors…
Part Number: TPS1211-Q1 Hi team,
When selecting a MOSFET for the TPS12110-Q1 used as an ideal diode, should the gate voltage level be logic-level, standard-level, or are both acceptable?
Part Number: TPS1211-Q1
Tool/software:
Hello,
Could you please share the distribution table data for V(BST_UVLOR) and V(BST_UVLOF)?
We can reach threshold levels in typical voltages and min/max from the datasheet but we need a distribution data…
Part Number: TPS1211-Q1 Tool/software: Hello Expert, Our customer is considering to use TPS1211-Q1.
Then, we'd like to make sure this device's behavior.
In normal operation, they will apply HIGH signal(approx. 3.3V) at EN/UVLO pin from MCU to turn…
Part Number: TPS1211-Q1 Other Parts Discussed in Thread: TPS1211Q1EVM Hello, I am designing a power distribution box for an automotive system. I have selected TPS1211/TPS4811 as controllers for several output channels to be overcurrent protected.
The…