Part Number: TPS1H200A-Q1
Hello,
I am designing the circuit used TPS1H200A-Q1.
This TPS1H200A-Q1 is planned to be used in HOLD MODE.
When used in HOLD MODE, if the output current becomes larger than the current setting value, it will be clamped at the…
Part Number: TPS1H200A-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 I am using two TPS1H200AQDGNRQ1 in parallel with 5A current limit setting (ie Rcl= 400ohms for 5A setting) on each to get 10A current limit option.
My input is 40/ 11A power supply and…
Part Number: TPS1H200A-Q1 Hi,
Customer designed Current Limit 2.5A in Holding Mode.
When the current limit is reached, the fault pin is low and the outpin voltage remains on/off.
It seems to correspond to Overload in Table 7-2. Fault Truth Table.
If the…
Part Number: TPS1H200A-Q1 Other Parts Discussed in Thread: TPS2HCS10-Q1 , TPS272C45 , TPS274C65 , TPS281C30 Hi team,
My customer is looking for a HS switch which has independent Vs pin. Use case is serilize two HS switch for redundancy protection, however…
Part Number: TPS1H200A-Q1 Hi Experts,
I am following the question about this one:
I want to describe the issue again, please see the test environment:
18V_PRI is input voltage to TPS1H200A
18_SEC is the output voltage of TPS1H200A
IN is the IN of TPS…
Part Number: TPS1H200A-Q1 Hi Experts,
TPS1H200A-Q1 is under evaluation on customer side. There are several issues occur on customer side, could you help on those issue? Thanks.
When the device is Latch-off mode, when the overcurrent occurs, it takes…
Part Number: TPS1H200A-Q1 Hi team,
My customer are using TPS1H200 HSD in our project, I have some question regarding the diagnostic.
From below table, after DIAG_EN pin is enabled,
Pin IN, we can control by our IOC;
Fault Pin: we can read out by our I…
Part Number: TPS1H200A-Q1 Hi,
what is the maximum current limit threshold that TPS1H200A can offer with external resistor? for example, can i set it to 10A if i use an external resistor ? Thank you!
Part Number: TPS1H200A-Q1
Why does the Fault signal occur when the current swings as shown in the above result for the TPS1H200A-Q1 IC?
Is it because of current limit exceed due to inrush current?
There is no information in the datasheet. What could…