Part Number: TPS1HB08-Q1TPS1HB08-Q1.pdf
TPS1HB08-Q1 is use to drive 12v/10A to infotainment system in automotive
Kindly please review the schematics share the feedback
Part Number: TPS1HB08-Q1 Hi team,
For HS switch like TPS1HB08, TPS2HB16, how to understand Imax parameter in the product folder? The Imax of TPS1HB08 is 10A, why current limit can up to 70A? Thanks!
BR
Jiawei
Part Number: TPS1HB08-Q1 Other Parts Discussed in Thread: TPS27SA08-Q1 Hello team,
TPS1HB08-Q1 datasheet doen't have the package dimension. Would you please share it?
Thanks,
Sam Lee
Part Number: TPS1HB08-Q1 Hi team,
If we connect ILIM to GND and we met reverse battery issue, will there be any reverse current pass through ILIM pin? Thanks!
BR
Jiawei
Part Number: TPS1HB08-Q1 Hi team,
What is the coplanarity and warpage of this device? There is a 3D picture in the datasheet, I can't get this information.
B&R
Lijia
Part Number: TPS1HB08-Q1 Hi team,
How much ICL min/max @ILIM=open for TPS1HB08 B QPWPRQ1? If it has valiation depending on TJ, could you disclose ICL min/max spec for each TJ=-40, 25, and 150C?
Regards, Ochi
Part Number: TPS1HB08-Q1 Hello!
Is it acceptable to open the SNS pin of TPS1HB08 if the diagnostic function is not used?
What are the concerns with leaving the SNS pin open?
Like the SEL1 pin, does reverse battery protection not work if the SNS pin is…
Part Number: TPS1HB08-Q1 Hi team,
How much current limit min and max spec are @ILIM=open with TJ=-40, 25, and 150C?
We use TPS1HB08 B QPWPRQ1 and datasheet says ICL = 104Atyp, but there is no information for min/max. If there are separated spec among TJ…
Part Number: TPS1HB08-Q1 Hi team,
We want to make reverse polarity protection. Is "Reverse ground current, IGND = -50mA" maximum allowable reverse current?
Do you recommend 1-kohm as RGND for both of TPS1HCxx-Q1 and TPS1HBxx-Q1 for "Figure 2…
Part Number: TPS1HB08-Q1 Hi expert
For TPS1HB08, continuous load current is 11A but current limit threshold is 77A. How to understand this two parameter? Whether is device can bear 11A continuous current and 77A peak current?