Part Number: TPS1HB08-Q1 Hello Team,
Can we connect the NC pins (12 - 13, 15) to the ground rather than keep it floating? What will be the effect on the device?
Regards,
Renan
Part Number: TPS1HB08-Q1 Hi team,
My customer is using TPS1HB08A-Q1 in their application for 16A as high side switch for power amplifier.
the load current is only about a few hundred mA but the Vout of TPS1HB08-Q1 is 0V after powering up. This happen in…
Part Number: TPS1HB08-Q1 Hello team,
About the Thermal Considerations about HSS such as TPS1HB08-Q1, I only see the Rds(on) at max temp. But if we use HSS at 1kHz frequency, how can we calculate the switching loss of MOS when in thermal consideration?…
Part Number: TPS1HB08-Q1 Hi team,
Customer has a question about the current through SNS pin when the load is disconnected.
When the load is disconnected, does 1uA(max) of ISNSleak flow through SNS pin in the condition of VDIA_EN = 5V or 0V?
Regards,
S…
Part Number: TPS1HB08-Q1 Hi!
The datasheet for this IC says, that the user can connect the SNS-pin parallel to several TPS2HBXX, all SNS stay on Hi-Z remain until the one of them is selected. But, for example, the error occurs in the control microcontroller…
Part Number: TPS1HB08-Q1 Hi team,
Could you tell me which pocket quadrant shown in TAPE AND REEL INFORMATION is on TPS1HB08AQPWPRQ1 pin1?
Regards, Ochi
Part Number: TPS2HB16-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 Hi TI
I use TPS2HB16AQPWPRQ1 / TPS1HB08AQPWPRQ1 in my design.
When R ILIM = GND, open, or out of range, its maximum current limit is a typical value in datasheet description.
I want to know…