Part Number: TPS1HB16-Q1 Hi Team - customer question below:
If the ILIM pin is left open, the device will switch to it’s internal current limit. Previous analysis also stated that a fault indication on the SNS pin would be set in this scenario but I…
Part Number: TPS1HB16-Q1 Other Parts Discussed in Thread: TPS1H100-Q1 , TPS2H160-Q1 I have an application where some devices downstream of our TPS1HB16A-Q1 smart high side switches have large input capacitances (50-100 uF). As expected, when attempting to…
Part Number: TPS1HB16-Q1 Hi TI team,
To better size the sense resistor for TPS1HB16-Q1 , I would like to know the maximum current from the sense pin. My assumption is the following:
ISENSE(max) = ISENSE(fault) = 5.3mA
This means that the current from sense…
Part Number: TPS1HB16-Q1 Other Parts Discussed in Thread: TPS272C45 What is the current consumption of the device, in case it is active, with for example VBB = 12 V, VOUT = 12V, VEN = 5V but VDIAG_EN = 0V? The datasheet states IDIA with VEN = 0 V, VDIA_EN…
Part Number: TPS1HB16-Q1 Hi Team,
I was looking through this devices datasheet and noticed the below portion in the current limit section of the d/s.
If I was performing a worst-case circuit analysis for the power dissipated within the device, would…
Part Number: TPS1HB16-Q1
Hi Expert,
Our customer uses TPS1HB16A-q1 in their project. They have some question about the current settings. Actually the max current 3.8A. So they choose Rilim=25K. In datasheet, the corresponding current limit threshold…
Part Number: TPS1HB16-Q1 Other Parts Discussed in Thread: TPS1HA08-Q1 , TPS1HB08-Q1 , TPS1HB35-Q1 Hi team,
Could you advise how to calculate the maximum ambient temperature for 8.5A continuous current for TPS1HB16-Q1 or TPS1HB35A-Q1?
It is described in…
Part Number: TPS1HB16-Q1
Hi Expert,
Our customer uses TPS1HB16A-q1 in their project and you can see the schematic as below. They have one problem.
In datasheet, we recommend that, for low-pass filter for ADC input, we recommend cap value between …
Part Number: TPS1HB16-Q1 Hi Team,
My customer wants to use the temp sense function of this device to provide an over temp shutdown pre-warning, but looking at the EC tables specs on I SNST it seems that there is some pretty big overlap in min/max:
Is it…