Part Number: TPS1HB16-Q1 1.SNS
When output overcurrent happen,Vout is shutdown.
After this, what information SNS pin indicate ?
2.Power on sequence
After VBB is applied,Do other input pins have any power on sequence ?
If you have reccomend power on sequence…
Part Number: TPS1HB16-Q1 Hi team, I'd like to calculate the current limit. However, I can't know how to calculate min to max. Could you tell me about the calculation method? I want to set 3.8A as the minimum value. Sincerely. Kengo.
Part Number: TPS1HB16-Q1 Questions:
1. If the battery is reversed, there is nothing in the TPS1HB16AQPWPRQ1 to prevent reverse current. Section 9.3.1.4 suggests using reverse blocking FET or Diode, which to an extent defeats the purpose of using the TPS1HB16AQPWPRQ1…
Tanmay,
For the integrated high-side switch devices, please refer to the following table:
Part Number
Channels
Ron (mΩ)
Imax (A)
Current limit (min) (A)
Current limit (max) (A)
TPS2H000-Q1
2
1000
0.75
0.05
1.3
TPS4H000…
Florian,
For the TPS1HB16-Q1 the capacitance between the VBB and ILIM pins is going to be very critical here and even trace capacitances in the line from the TPS1HB16-Q1 to the microcontroller would cause the current limit to not behave properly. For…
Part Number: TPS1HB16-Q1 Other Parts Discussed in Thread: LM5060-Q1 Hi,
My customer has the following requirements for an automotive load switch:
Vin = 10-16V
Iout = max 6A for 20ms, nominal 3.5A
I suggested the TPS1HBxx-Q1 family…
Part Number: TPS2HB35-Q1 Other Parts Discussed in Thread: TPS1HB35-Q1 , TPS1HB08-Q1 , TPS1HB16-Q1 Hi Team,
Customer wonder if TPS2HB35-Q1 / TPS1HB35-Q1 / TPS1HB08-Q1 / TPS1HB16-Q1 can support ASIL-B?
I saw we have Functional Safety document, but not showed ASIL…
Part Number: TPS1HB16-Q1 Hi Timothy,
I have a question regarding the TPS1HB16AQPWPRQ1 chip. Would tying the Enable and Latch pins together and toggling them simultaneously allow us to clear the fault? Or do we need to power cycle the circuit to clear…
Part Number: TPS1HB16-Q1 Hello,
I am planning to use a Smart High Side Switch like the TPS1HB16-Q1 ( https://www.ti.com/product/TPS1HB16-Q1 ) in a product to drive and protect different loads as seen in the figure below.
I know it is AEC-Q100 qualified f…
Part Number: TPS1HB16-Q1 Hi Timothy,
Thank you for the quick reply and for pointing out the increased current consumption.
One other question we have is if it would be okay to tie ENABLE and LATCH together?
Thank you,
Neal