Part Number: TPS1HB16-Q1 Other Parts Discussed in Thread: TPS2596 , , TPS1HB50-Q1 , TPS1H100-Q1 Hi all
My customer has USB Type-C ports (sink) where he wants to implement a 1A or 3A current limit, ideally resistor adjustable.
Although he is only using 5V…
Part Number: TPS1HB16-Q1 Is it okay to just pull the DIA_EN pin high and still be able to use the diagnostic functions of the chip. We don't have enough pins left on our microcontroller and want to make sure the part will still work correctly if we do…
Part Number: TPS2HB35-Q1 Other Parts Discussed in Thread: TPS1HB16-Q1 Hi Team,
We are considering if we can apply TPS2HB35's dual channels as a single channel? Would that be workable theoretically? Anything we need to pay attention when we design? …
Hi Matthew,
All our high side switches include a VDS clamp that clamps the output voltage to the specified value during inductive turn off events. We also offer current limiting either with clamping or immediate turn off. For a single channel 20mOhm…
Part Number: TPS1HB35-Q1 Hello, after the helpful recommendation in this thread: e2e.ti.com/.../tps1hb16-q1-capacitive-load-driving
I am now testing using TPS1HB35 C -Q1 in the circuit instead. It appears to be working well for this application, however…
Hi Danilo,
In addition to the eFuse recommendations, what are the protection features required on the output side?
If the protection required is minimal, then a load switch like TPS22810 could work. If more features like ability to drive external inductive…
Part Number: TPS1HB08-Q1 Hello!
I want to get AEC-Q100-012 Short-Circuit Reliability Test Results of below parts.
I checked document "SLVA709A" but the desired parts was not on it.
TPS1HB08
TPS1HB16
TPS2HB16
TPS2HB35
DRV9810
DRV8244
Regards…
Part Number: TPS1HB08-Q1 I want to get Latch-up Test Results(e.g. AEC-Q100-004D , JESD78E) of below parts.
The customer requires that test results must be submitted.
Otherwise they may not approve the use of the TI parts.
TPS1HB08
TPS1HB16
TPS2HB16
…
Part Number: TPS4H160-Q1 Other Parts Discussed in Thread: TPS1HB50-Q1 , TPS1HB16-Q1 , TPS22810-Q1 Hello,
my customer is looking at driving some solenoid valves with a load current of 1.5A max using our TPS4H160-Q1 and would like to know what is the maximum…