Part Number: TPS2113 Dear Sir I am designing a circuit using TPS2113. It is a general circuit configuration that normally operates on a battery and charges when an AC adapter is connected. The "STAT" signal is detected to detect that the AC adapter is connected…
Part Number: TPS2113 If the tps2113 IN1/IN2 input voltage is the same(from EN=0, VSNS=0), what happens to the output? AND I'm looking for a device that uses IN1->IN2 sequentially, not outputting a high voltage value, available without any control such…
Part Number: TPS2121 Other Parts Discussed in Thread: TPS2113 , Hi Sir,
My customer is using TPS2113 on their previous generation platform and seeking our advise if we have a newer solution for them.
I propose TPS2121 to them, but on the spec, TPS2121 have…
Hi PMRC,
Do you mean TPS2113? I'm finding a TPS2216 but not TPS2213.
Understood about priority mode not being an option. There's also TPS2121 which has a much higher hysteresis of about 300mV typ, but has an Iq of about 300uA. TPS2115A has a hysteresis…
Part Number: TPS2113 Other Parts Discussed in Thread: BQ24075 , , , TPS22912C
We are using TPS2113DRB unit as a power mux. EN# is tied to VSS, ILIM is tied to VSS with 400 Ohms. IN1 and VSNS are tied to USB_5V supply. IN2 is tied to a battery charger's…
Part Number: TPS2113 Other Parts Discussed in Thread: TPS2120 , Hi E2E,
we would like to use the TPS2113 in an environment where IN1 is connected to a DCDC converter (2.5A) and a Li-Ion battery on IN2. The output drives a CPU someperiphals and a GSM modem…
Hi Patrick,
Looking at the VOUT waveform above, the starting voltage is 0V. After enable, the output voltage is maintained.
It consists of TPS2113->BUCK-BOOSTER->LOAD(1A).
If vsns is maintained, operation can be confirmed like a table.
When VSNS…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2113 When Vin1(V_5V_S) goes power down, there is a rining on OUT(V_BAT_4V) of TPS2113.
Is that the normal in TPS2113.
Customer is looking for a solution for voltage switch OUT=IN1/IN2 bease on the…