Part Number: TPS2115 Other Parts Discussed in Thread: TPS63000 , , , TPS2121 Dear TI-Team,
we have a total of three power sources: USB (when debugging), PV (with small buffer battery) and a large li-ion battery. TPS2115 selects between PV and battery, after…
Part Number: TPS2115 Other Parts Discussed in Thread: TPS22976 I'm looking for a recommendation. I have two power rails, nominally 5V each. I want to be able to switch between them with 1 GPIO pin. Total load current is 6A max. I've had good results …
Part Number: TPS2115 Other Parts Discussed in Thread: TPS65217 , , Hello,
In our power architecture we have TPS65217 and TPS2115 .
We use TPS65217 to switch between AC and USB but the load is only AM355x processor and DDR.
But for the peripherals ( as load…
Part Number: TPS2115 When the load is exceeding the current limit protection, what is the beahvior of the device ?
Is the devcie latched in OFF state and the output is kept OFF ?
or
- once current limit is exceed the internal mosfet is driven in linear…
Part Number: TPS2115 Hi all There is a following explanation at the terminal functions table in the datasheet P7. " Each pin has a 1-µA pullup resistor." Please tell me the value of pull up resistor? Best Regards, Sho
Part Number: TPS2115 Hi Team, The datasheet shows the following TRUTH TABLE. Is it possible case that Q1(IN1-OUT switch) and Q2 (IN2-OUT switch) are both on under specific conditions? If the answer is yes, I would like to know the condition. Best Regards…
Part Number: TPS2112 Other Parts Discussed in Thread: TPS2115 , TPS2114 , TPS2113 , , TPS2116 Hi team,
The datasheets of TPS2112, TPS2113, TPS2114 and TPS2115 show that the Eco-plan of below devices are TBD.
TPS2112PWRG4
TPS2113PWG4
TPS2114PWG4
TPS211…
Other Parts Discussed in Thread: TPS2115 I have a current consumption problem with the TPS2115. It draws 400uA from IN1 while it draw only 40uA from IN2 as expected.
I’m using the TPS211xEVAL configured on Auto switch, I plug a power supply with 3.6V to…
Other Parts Discussed in Thread: TPS2115 I am using the TPS2115 to switch between an always on linear supply (IN2) and a switched 5V source (IN1). Here is a snippet of the schematic:
When the switched source is ON, the D0 input is high - when the switched…
Other Parts Discussed in Thread: TPS2115 Hello,
I would like to know if it is possible to add a TPS2115 5V autoswitcher from TI to a Power architect design in Webench. Our design needs to switch between two 5V regulators and we would like to know if it…