Part Number: TPS2115A-Q1
Tool/software:
Hi, Support Team
We will use TPS2115A-Q1, schematic as below chart.
have any concern?
schematic:
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TPS2115A-Q1 Hi Team,
Let me ask two quick questions. 1. Could you tell me the background why this device's operation range is limited up to 85C? 2. What kind of list will be estimated if the device will use in 100C ambient condition?
My…
Part Number: TPS2115A-Q1 Other Parts Discussed in Thread: TPS2115A Hi,
I m looking for a low cost ORing solution (automotive qualified) that can be used for 5.V rail.
i.e. I have two sources of 5V and I need provide output to the load from any one of them…
Part Number: TPS2121 Other Parts Discussed in Thread: TPS2115A-Q1 Automotive Grade TPS2121?
Any equivalent to the TPS2121 or similar automotive grade component? other than TPS2115A-Q1, I need help connecting 2 power supplies (Master-slave), one 12V (master…
Part Number: TPS2121 Other Parts Discussed in Thread: TPS2115A-Q1
Automotive Grade TPS2121?
Any equivalent to the TPS2121 or similar automotive grade component? other than TPS2115A-Q1, I need help connecting 2 power supplies (Master-slave), one 12V (master…
Part Number: TPS2115A-Q1 Other Parts Discussed in Thread: TPS2115 We are using TPS2115 Power Mux to power a micro-controller dev-board. The circuit schematic is shown below.
Here we are implementing manual switching feature in order to select the input…
Hi Manikumar,
Yes, I agree that what you described is the expected behavior of using two similar input voltages.
Understood that the suggested parts are not auto qualified - I missed catching that. How about TPS2115A-Q1 , power mux, or 2x TPS22953-Q1 , which…
Part Number: TPS2115A-Q1 Hi team,
May I know if TPS2115A-Q1 current limit can be set to 2A? (ILIM = 249 ohm)? As I saw in datasheet, the maximum is 1.25A.
If it can't be set to 2A, may I know the reason of it?
Thank you.
Regards,
Allen
Part Number: TPS2115A Hi
USB POWER SWITCH ( adjustable current + OVP ) Requirements: Regardless of whether it is turned on or off, it must have a reverse cut-off function to prevent reverse backflow USB PORT can be used alone and only needs 1.XA curren…