Part Number: TPS2000E Other Parts Discussed in Thread: TPS2553 , TPS2115A-Q1 Hi
USB POWER SWITCH ( adjustable current + OVP ) Requirements: Regardless of whether it is turned on or off, it must have a reverse cut-off function to prevent reverse backflo…
Other Parts Discussed in Thread: TPS2115A , TPS2115A-Q1 , TPS2115 Hi team,
My customer has a few questions for Settling time of TPS2115A(TPS2115A-Q1).
1. Is settling time a period from detection over current to protect operation ?
2. What values for…
Other Parts Discussed in Thread: TPS2115A-Q1 Hi,
I want to check TPS 2115A-Q1 with SPICE, but I can not find a model. Is there a SPICE model?
Best Regards,
Other Parts Discussed in Thread: TPS2115A-Q1 Hi
I want the +/-1 sigma value and median value for "Hysteresis of IN2-IN1 comparator" of TPS2115A-Q1.
Could you share me them?
If needed, I want to communicate directly.
BestRegards
Other Parts Discussed in Thread: TPS2113A Hi,
My board has 2 usb 5V inputs.(1 from USB port and another from USB wall Charger)
I plan use USB port to power my board for most of the time and use charger as a back up if more current is needed.
The auto…
Other Parts Discussed in Thread: TPS2115A-Q1 Hello, I have a question about TPS2115A-Q1.
SWITCHING CHARACTERISTICS of tr "Output rise time from an enable".
The page-6 of SBVS124 describes only the value at Ta=25℃. MIN = 1.0ms TYP = 1.8ms MAX =…
Other Parts Discussed in Thread: TPS2115A-Q1 , TPS2115A We are working in a solution for power multiplexing, and we want to use TPS2115A-Q1. The truth table in datasheet is not the same as in TPS2115A. It seems that D0 and D1 are swapped, is this correct…
Other Parts Discussed in Thread: LP5900 , LM74610-Q1 , LM66100 , TPS2115A , TPS2121 , TPS2120 Hello,
for an upcoming project of a portable device that has the possibility to be connected to an USB 2.0 host system I want to implement a power supply OR-ing scheme…