Part Number: TPS2116 Hello,
In the circuit below, I switch between the 5V input of VIN1 and the USB VBUS of VIN2.
The operating mode is priority mode.
I am currently experiencing the following symptoms.
1. When VIN1=5V input and VIN2=floating, the same…
Part Number: TPS2116 Other Parts Discussed in Thread: BQ24081
Hi team,
I'm working on a li-ion battery powered device which can run from USB when the battery is discharged. I have selected the TPS2116 to switch between the battery and USB power. …
Part Number: TPS2116 Other Parts Discussed in Thread: TPS2117
Hi,
I'm using the manual mode with this chip, that both MODE and PRI1 are toggled by GPIOs. And I have several questions:
May the IO signal level higher than both VIN1 and VIN2?
I'm considering…
Part Number: TPS2116 Hi,
I have 3 questions. Could you please advise us?
*1.
My customer considers using TPS2116DRLR with the following connection.
Mode pin : connect with VIN1 pin (Manual Mode)
VIN1 pin : 3.3V Power
VIN2 pin : 1.8V Power
PRI1 pin :…
Part Number: TPS2116 Dear Sirs,
for a very important project of ours, the customer is asking us the Mean Time Between Failure (MTBF) value for the p/n TPS2116DRLR
Could you please provide to us this data? Thanks on advance
Part Number: TPS2116 Hi,
we need to supply our product from three possible power sources: - Lead acid battery with solar charging (the output voltage can reach maximally 4.7V when charged). - Lithium Thionyl Chloride (Li-SOCl2) primary cell (the output…
Part Number: TPS2116 We are currently in need of a step down converter + power selector IC for our current project. Could you please let us know if such an IC is available from TI?
Part Number: TPS2116 Hi team,
Customer wants to know the On-Resistance when the Iout=1A.
Can you share the TYP and MAX of the On-Resistance when Iout=1A as in the Datasheet?
Best regards,
Foong Wei Seng
Part Number: TPS2116 Other Parts Discussed in Thread: TPS2121 I am currently trying to perform simulations using the TPS2116DRLR. The primary voltage is 3.3V and the secondary is 3V. I currently have the device set up in primary switchover mode where the…