Part Number: TPS2116 Power switching is performed using TPS2116DRLR. PR1 is set to "H" and VIN1 is used with priority.
If you turn off VIN1 while using VIN1=5V, VIN2=0V, it seems that the current flows backwards to VIN2.
I understand that…
Hi Martin,
Thanks for your patience as I have been out of the office this past week due to the US holiday.
Great to hear that you found the solution! I saw that IN2 looked stable and undisturbed in your waveforms so IN2 capacitance didn't look like an…
Part Number: TPS2116 Hi Team,
I have concern regarding this power path changing IC. In my application we have Vin1 connected to 4.2V (PR1 is connected to Vin1 vias Resistor divider and Mode is directly connected to Vin1). My Vin2 is connected to 4V battery…
Part Number: TPS2116 Hi TI Teams,
We have some question about the priority mode of TPS2116, the details are show as below:
1) Does the PRI have a delayed comparison function? Due to the influence of the internal resistance of the core, the voltage of light…
Part Number: TPS2116 Hi experts,
The datasheet specifies that the maximum value of VIH, MODE is 5.5V, but is this correct? If this is true, the MODE High threshold will vary by as much as 4.5V. Also, as far as I read other parts of the datasheet, I read…
Hello,
We do not provide specific SOA curves; instead we recommend operation within the recommended operating conditions with the possible exception of short transient events.
This means we do not recommend driving >2.5A on a DC basis. We are releasing…
Part Number: TPS2116 Hi Experts,
Our customer would like to know the behavior of the TPS2116 when is power supplied and it has a temperature lower than -40°C.
Is there any derating curve versus temperature?
Thank you and best regards, Gerald