Hello Shreyas,
we tried ordering for EVM free samples with the links which you have shared, but we are not authorized to get free samples. is there any alternate way of ordering.
Thanks for suggesting TPS2121, we have ordered 2 no's of component for testing…
Part Number: TPS2120 Hello!
Section 9.3.6 of the datasheets says that reverse current blocking for TPS2120 is triggered by VIRCB, but only IRCB is defined. And, IRCB can be up to 2A max as shown in the electric characteristics of the datasheet.
Does…
Part Number: TPS2120 I am using the TPS2120EVM and notice that the device becomes unstable during a certain condition:
I am using the 5V inputs configuration, with the jumpers set as follows:
Connector Label Position
J1 PR1…
Part Number: TPS2120 Hello,
again on the TPS2120, this component is powered when the full product is in stand-by mode,
in the case we have no load on IN1 and 7V (battery) on IN2 and we have a small load on output, what would be the leakage current ?
…
Part Number: TPS2120 Hello,
we are using the TPS2120 to select between two 12V and the OUT might in some cases be linked to a 15V source,
is the RCB (reverse current blocking) protection work in this case, are the inputs protected ?
Thank you,
Best regards…
Part Number: TPS2120 Other Parts Discussed in Thread: TPS2121 Hello,
I contact you back concerning a problem we have with our TPS2120 which is configured in automatic mode between a 12V external and 7V battery.
When we unplug the external 12V, the system…
Hi Tommy,
This recommendation is common to both TPS2121 and TPS2120:
We also recommend that the CSS capacitor is positioned close to the device to avoid any parasitic effects on the rise time.
For these ball grid array packages we have the following…
Part Number: TPS2120 Other Parts Discussed in Thread: TPS2121 Hi,
We are using TPS2120 (2:1 Power MUX) with two 5V power sources at IN1 and IN2. PR1 pin is shorted to IN1 and we are not using OV1/OV2 (both grounded).
When the system is first turned on…
Part Number: TPS2120 Other Parts Discussed in Thread: TPS2124 The TPS2120 does not appear to have a dedicated enable pin. Is there any way to disable the output? I am thinking I could perhaps manipulate the OV1 and OV2 pins. If I were to drive both OV1…