Part Number: TPS22918-Q1 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the replacement of TPS22918-Q1
Please help suggest a newer IC, THX
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: TPS22918 Hello,
I have following schematic:
The transistor at ON pin is not populated and CT=100p.
And I get following measurement:
I'm surprised that level at ON pin go to ~2,6V when IN is 1…
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: ADS7138 , TPS22918 The switch device of TPS22918 is used for switching of AVDD power for ADS7138 ADC IC, in the signal measurement block circuit of a control PCBA project, simplified circuit diagram…
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: TPS22918
Hi,
ESD rating values of TPS22918-Q1 and TPS22918(nonQ1)'s are different on the specification.
Is this difference caused by certification?
Are these the save actual tolerance?
Best…
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: TPS22918 Hello Team,
My customer consider using TPS22918-Q1 for SoC power sequencing at ADAS camera application and he asked us to provide the application schematic for 1.8V VIN and 0.5A Output…
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: TPS22918 Hi team,
My customer is using TPS22918-Q1 and complaining that they have a too-long 2ms delay time. According to their application(Vin=3.3V, Cct=1nF) I found the typical values of td=590us…
Part Number: TPS22918-Q1 Hi,
PIN3 ON, What is the threshold voltage for opening and closing ?
This PIN is externally connected to the control chip, so we want to see whether the specific value of threshold voltage of high and low level matches.
Thanks…
Part Number: TPS22918-Q1 Hi team,
I’d like to confirm below sentence in the datasheet of TPS22928-Q1.
In case that 30uF capacitor are used at the input path of the other device after the output of TPS22928, should the input capacitor still be…
Part Number: TPS22918-Q1 Hello Team,
we found in datasheet 'SLVSCZ8A –JULY 2016–REVISED JULY 2016' information which do not fit.
Chapter 8.3.3 - Equation 3 is used pF unity for CT cap and Table 2 shows 220pF@5V for rise time 650us. …