Part Number: TPS22920 Hi team,
My customer use TPS22920 in their project. Below is their schematic.
The test waveform as shown below.
According the datasheet, when the ON signal is low, the Vout will be low. But the test result show the Vout start going…
Part Number: TPS22920 Hi,
I'll be using this load switch, but a question came to mind when I was reading the datasheet.
The board I'm designing is powering-up a device under test. So I added the TPS22920 to protect the regulator when turning…
Part Number: TPS22920 Dear :
The TPS22920YZPRB device has a backside coat, TPS22920YZPR is not, what effect is the difference between TPS22920YZPRB and TPS22920YZPR ? in design application, can the both be pin2pin instead ?
Part Number: TPS22920 Hi all,
Would you please helping to provide CB/UL report about TPS22920YZPR for my customer? And, do we have IEC 62368-1 version?
Regards,
Gary Teng
gary.teng@arrowasia.com
Part Number: TPS22920 HI,
My customer has been using TPS22920YZPRB and now ordered TPS22920YZPR (both are on the AVL) due to better availability.
Their manufacturing department is worried because the color of the package is different:
TPS22920YZPRB is…
Part Number: TPS22920 Hi team,
customer would like to use TPS22920.
Would you please review schematic/layout and provide your comment?
Thanks for help!
BR,
SHH
Part Number: TPS22920 Hello,
My customer is facing a couple of issues at TINA transient analysis as follows.
At TPS22920_old_sch.tsc, VIN oscillates as framed with RED circle.What’s wrong?
TPS22920_old_sch.tsc
And at TPS22920_new_sch.tsc, my…
Part Number: TPS22920 We are trying to use TPS22920 load switch (and also tried TP22970 with the same results) to limit inrush current into our SFP+ module. When the module is first plugged in into a powered host board (Switch) it creates multi Amp spike…
Part Number: TPS22920 Other Parts Discussed in Thread: TINA-TI Hello,
At TPS22920 TINA-TI Transient Reference Design, what is the RDSON highlighted in RED in the following transient plot?
How can users modify its parameter if required?
Best regards…
Part Number: TPS22920 Hi,
I have an application with a high capacitive load of 2000uF sitting on a plugable board. Main reason for the 2000uF is that the board can be unblugged and the power need's to stay up and running so that the supply can run a…