Dear Rakesh
Sorry. It's my misunderstanding. If 3A current and needs emulated diode, how about TPS22920? Or TPS25942A is only suitable solution for requirement. Thank you.
BR
Patrick
Hi Steve,
The TPS22990 is the lowest on-resistance load switch we have. Is the issue that the VBIAS min for the device is greater than 2.5V - 5%, or that the on-resistance is above 4mΩ? Also, is it 4mΩ max or typical on-resistance?
Another…
Other Parts Discussed in Thread: TPS22920 , TPS2420 , TPS2590 , TPS25910 I have an application where I would like to enable a series load switch with logic control and controlled turn on but need to be able to pass single voltages from 3.3V to 15V DC. is…
Other Parts Discussed in Thread: TPS22964C , TPS22967 , INA230 , INA231 , TPS22920 Hi,
Iam looking for CAD/bxl files for
tps22964c
tps22967
tps22920L
ina230
ina231
Can someone please help me with a link to these. (I searched the CAD files webpage)
Thanks…