Part Number: TPS2419 Hi,
Assume
Vbus1 = 12V and Vbus2 = 5V
Case: When EN pin of Vbus1 controller is pulled low
The load will still see Vbus1 voltage (12V) due to body diode conduction. Is this right?
If yes, what is the exact functionality…
Part Number: TPS2419 Other Parts Discussed in Thread: TPS2410 Dear TI!
I decided to use your TPS2410 in a dual power supply application. I made the schematic attached below. My problem is the following: when both of the power supplies are connected…
Part Number: TPS2419 Other Parts Discussed in Thread: TPS2412 Dear Sir/Ms.
TPS2419 test circuit, when V1 OFF, V2 ON, VA will be about 1~2V, why is this happening, is it a problem of IC itself?
Best Regards,
Kami Huang
Part Number: TPS2419 Hi
My customer is using TPS2419 to combine 1 1 redundant power supplies. when these two power supplies are working, there are whistlers from power supplies. If we turn off any of them, the whistlers will disappear. The specifications…
Part Number: TPS2419 Other Parts Discussed in Thread: CSD17577Q5A , CSD17577Q3A Dear Team,
My customer would like to use TPS2419, do you have suitable MOS for 12V/9A?
BR
Kevin
Part Number: TPS2419 Dear TI,
We are currently designing a N+1 Redundant Power Supply.
With the schematic as it is, (RSet = 35 ohm) we are able to get the power supply functioning properly when both Power Supplies are connected. However if…
Part Number: TPS2419 Hi team,
customer using TPS2419 on their system, but they found when they input 12V on C pin, they could test 10V on A pin, and up to 20V on BYP pin. Nothing change when they pull up or pull down EN pin.
Could you please help…
Other Parts Discussed in Thread: TPS2419 , TPS2411 , TPS2413 Hi All:
We are now designing a product with DC power supply. We choose TPS2419 to manage the backup battery supply .So that TPS2419 will driver the N-MOS to swith on the battery supply when…