Part Number: TPS25200 Other Parts Discussed in Thread: TPS2595 , TPS25961 Hi everyone, The TPS25200 eFuse is used in our design for overcurrent and overvoltage protection with the features of the IC. But the IC features the UVLO at 2.35V. To implement…
Part Number: TPS25200-Q1 TPS25200-Q1: Parameters for worse case analysis - Power management forum - Power management - TI E2E support forums Hi Team,
Based on the previous discussion, we would like to inquire about the rise time when COUT is 12.1…
Part Number: TPS25200 Tool/software: Hi,
I'm trying to use the TPS25200 for current limit.
For example:
1. I want to limit the current to 500mA so according to equation 5 on page 17 under section 9.2.2.5 "Design Below a Maximum Current Limit"…
Part Number: TPS25200 I am sharing the power section of my design for review and would appreciate engineering feedback on whether the architecture is valid and likely to operate reliably in practice.
The +5 V rail feeds a TI TPS25200DRVR current-limited…
Part Number: TPS25200 Hi team,
Does the FAULT pin remain an open-drain output even when the device is disabled (EN is Low)? Or does the FAULT pin go Low when the device is disabled?
Sincerely, Goto
Part Number: TPS25200 Hi team,
May I know if this IC supports dynamic current limit?
Customer would like to change the external RILIM value while EN=High. Below points are important to the operation of this end equipment.
RLIM decrease while EN…
Part Number: TPS25200-Q1 Tool/software: Can I connect the "~Fault" pin to "Enable" pin in order to lockout disconnection mode when fault appears first time rather then re-try mode?
Part Number: TPS25200 Other Parts Discussed in Thread: TPS25947 , TPS2552 , TPS2661 , TPS2640 , TPS2662 Tool/software: Hi,
We are using the TPS25200 eFuse with reverse current blocking in our product design. However, there are instances when the current…
Part Number: TPS25200 Tool/software: Hi Team,
Could you please advise does TPS25200 have IEC 62368-1 certificate?
If not, could you please recommend a alternative solution of TPS25200 that has IEC 62368-1 certificate?
Best regards,
Terry