Part Number: TPS25200-Q1 Other Parts Discussed in Thread: TPS629210-Q1 , TPS552882-Q1 Hellow,
I'm using the TPS25200-Q1 three times in my board. Twice for 3.3V switching and once for 5V switching.
TPS629210-Q1 feed power to the 3.3V switches. A se…
Part Number: TPS25200 We would like to ask about the accuracy of the current limit threshold for eFuse TPS25200.
The data sheet contains formulas to calculate IOSmax and IOSmin when 1% tolerance is used for RILIM, but I think these formulas will also…
Part Number: TPS25200 Other Parts Discussed in Thread: TXU0101 Hi!
In my device I plan to use 5V pin as input and output depend on situation.
Device is lipo battery operated
- Input current limit 300mA. Should always provide 5V to the system if present…
Part Number: TPS25200-Q1 Other Parts Discussed in Thread: TPS22950-Q1 Hi Team,
May I know whether the OCP mechanism/behavior of both TPS25200-Q1 and TPS22950-Q1 are the same or not?
Based on datasheet, the description is the same but demo waveform are…
Part Number: TPS25200 Hi,
We are looking at using TPS25200 to limit the input current in order to be compliant to IEC 62368 PS1 (I.e. below 15W) in a 5V device.
What happens in a single-fault condition for the Rilim and other necessary components?
Rilim…
Part Number: TPS25200 Hello,
Is there an additional current consumption of the eFuse when the input voltage is between the 5.4V and 7.6V ?
The datasheet only shows the current when the input is at its absolute maximum value of 20V, with the over voltage…
Part Number: TPS25200 Other Parts Discussed in Thread: TPS25961 during normal condition below circuit is only running under 5V.
in case abornal happens, it may short to 12V.
I would like to use efuse to protect circuit after efuse, please recommend part…
Part Number: TPS25200 Hi team,
Customer need a 3A max continuous support efuse part. They also need 0.5A ~3A dynamic current limit. TPS25200 get dynamic current limit feature. But current is 2A continuous max.
Could you help check about a more suitable…
Part Number: TPS25200 Hi team,
The datasheet states the min/max output current rating. Does this mean we need to sink/source current which is listed on the table? Or, is it OK to have very small (much smaller than the listed value) output current?
…
Part Number: TPS25200 Hello,
What is the connection when the "FAULTn" pin is not used in TPS25200?
1) Open
2) Pull up to VIN
3) Connect to GND
Thank you for your support.
Regards.