Part Number: TPS25200 Hi experts,
My customer is using TPS25200 as below schematic show. as you can see, there is a suspect voltage drop. I don't have a EVM on hand yet, and EVM user guide didn't show related test result. May I have your suggestion…
Part Number: TPS25200 Hi, Support Team
Customers are developing products using the TPS25200.
I am trying to not use the FAULT pin during development,
Can I just leave the pin as NC when not in use?
Or does it require separate processing?
Thanks.
Regards…
Part Number: TPS25200 Hi team,
If TPS25200 trigger OVLO protection during power on transient stage to turn off FET, but when input voltage reduce back to 5V, will MOSFET turn on again or keep turn off?
Please advise.
Thanks
Part Number: TPS25200 I am Koki Tsushima, who is FAA.
My account concerns that Is there possibility to act as following order.
1. Turn off
2. FAULT activated
I think this could be happed because when overcurrent was detected, the signal transit to FAULT…
Part Number: TPS25200 Hi team, Customer is using FPF2495 at Type C input protector, do we have any suitable part recommend for this function? Voltage higher at similar level ~28V, and WCSP package is preferred. Thanks.
http://www.farnell.com/datasheets…
Part Number: TPS25200 Other Parts Discussed in Thread: TPS2553 , TPS25221 Hi,
I'm in midst of migrating design from using TPS2553 switch to TPS25200 eFuse for USB charging port application. I do know that these are two different products but I would want…
Hi Saumil,
The TPS25200 clamps the output voltage with respect to its reference GND. Here as the IC GND is diode drop voltage above the system GND, the otuput voltage w.r.t system GND would be 5.55V + Diode drop
Do let us know if you have any other questions…
Hi Devipriya,
In eFuse, auto qualified we only have TPS25940-Q1, TPS25200-Q1.
Hotswap have timer pin which you can set to allow current transient. After timer only device will shut off.
Robust Hot Swap Design (Rev. A) (ti.com)
You can also check ideal…