Part Number: TPS25200 Other Parts Discussed in Thread: TPS25942A Hi team,
My customer is evaluating TPS25200. The normal input voltage is 5V. But the maximum transient input voltage can be as high as 21V. I noticed that in our TPS25200 datasheet, the…
Part Number: TPS25200 Hi,
do we have any characterization data on how the logic input threshold levels vary across temperature.
I have a customer that is looking at a design with very low margins, and they wanted to have a feel for the variation.
Thank…
Part Number: TPS25200 Hi
I got a question from my customer about TPS25200.
I think this device's Absolute Maximum Ratings of Voltage from IN to OUT is -7V ~20V.
If it is inputted reverse voltage of 5V at OUT terimnal on enable, are there the possible…
Part Number: TPS25200 Hi team,
My customer doesn't use nFault output. nFault pin doesn't connect anywhere in the customer's schematic.
I think the customer have to connect the pull down resistor to GND when they don't use. Is it correct?…
Part Number: TPS25200 Other Parts Discussed in Thread: TPS2595 Please help recommend the same features as the TPS25200, but at a lower cost for low-cost devices or new devices, thank you very much!
Part Number: TPS25200 Hi Team, My customer is requesting IEC60950-1-am2 recognition for the current limit. Do you have IEC60950-1-am2 recognition?
Regards, Ogasawara
Part Number: TPS25200 Hi, TI member,
We are surveying for TI/TPS25200DRVR and have below question.
Would you mind to help us for below question?
1. Could TI/TPS25200DRVR use for Vin/Vo:3.3V and Vin/Vo:5V?
2.If
Vin=3.3V, Vout=3.3V?
Vin=5V, Vout=5V?
3.If…
Part Number: TPS25200 Hi Team,
I would like to know because there is not enough understanding of the “8.3.3 Overcurrent Protection” part of the datasheet.
"The second condition is when a short circuit, partial short circuit, or transient…
Part Number: TPS25200 Hi Team,
Customer use TPS25200 in the usb protect circuit. Their output get large caps, the input cap is smaller compared with output cap. When they move away the USB input power, does it possible for the output discharge circuit…