Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS25772-Q1 , TPS25846-Q1 , TPS25762-Q1 , TPS25830A-Q1 Hello,
I selected TPS2549-Q1 for an OEM project but according to semiconductor assessment result it was classified as legacy technology in terms…
Hi Ziv
The customer has completed the hardware modification plan and precautions mentioned above, and the packet loss rate has improved to some extent. However, they still did not use Apple certified compatibility testing. Please help analyze the possible…
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS2549 , Hi
HI engineers:
I test USB eye diagram host mode fail with IC TPS2549-Q1,but if without TPS2549 USB eye diagram pass。how to improve this question?
Part Number: TPS2549 Hello,
I am looking to do a USB-A Dedicated Charging Port (DCP) and there are some parts from the datasheet that I am unclear on. For our application, we are looking to charge basic USB-A products with shorter cables (less than 3m…
Part Number: TPS2549 Other Parts Discussed in Thread: TPS2546 , TPS2547 Hello,
I am looking to do a USB-A Dedicated Charging Port (DCP) and there are some parts from the datasheet that I am unclear on. For our application, we are looking to charge basic…
Part Number: TPS2549-Q1 What type of USB port does this IC support. and can we moniter the Output voltage and current which is transfered to the portable device through the host?
Part Number: TPS2549-Q1 Hi, my customer has some questions about TPS2549-Q1.
1.When Vin=5V, EN pin is shut down, then the Vout pin is sunk into 5V voltage, will this damage the device?
2. When Vin hasn't powered on, EN status is not sure, then the Vout…
Part Number: TPS2549 Other Parts Discussed in Thread: TPS2546 , Hi Experts,
right now customer need to pass the MFI R31 OCP test on their headunit product,
in their current design they used TPS2546, but it can not pass the test.
Question:
1. does the TPS2549…
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: LM63635-Q1 , Hi
In my new design i have a USB port with power delivery for charging 5V @2.4A requirement . So i drafted the circuit by using TPS2549-Q1 and LM63635-Q1 , same is attached here for the…