Part Number: TPS2549-Q1 Hi team,
I have a question about power on sequence of TPS2549-Q1. Can you confirm if the following condtion is okay?
Sequence :
1. EN (3.3V) is enabled
2. VIN (5V) is powered
Thanks,
Sam Lee
Part Number: TPS2549 Other Parts Discussed in Thread: TPS2546 , Hi,
I would like to ask you about the TPS2549 device. (question 1) Set "001" in the DCP mode setting. The Current Limit Setting will be "Hi", but I will not use "Lo".…
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS2546-Q1 Hi team,
Why does he has divider3 instead of divider1 and divider2?
I found that TPS2549-Q1 and TPS2546-Q1 looks similar function but different DCP auto operation such as "Divider3 mode…
Part Number: TPS2546 Other Parts Discussed in Thread: TPS2549 , Hi team,
can the TPS2549 replace the TPS2546 directly in below application? only Pin 4 CS function is difference, can we replace TPS2546 without any hardware change?
thank you
Part Number: TPS2549 Other Parts Discussed in Thread: TPS51396A Hi,
As TPS2549 EVM figure, it only for this four DC/DC converter as red mark?
Or any used FB adjustable DC/DC converter? I used TPS51396A is ok, right? thanks!
Jeff
Part Number: TPS2549-Q1 Other Parts Discussed in Thread: TPS2546-Q1 Hi TI-team
My customer wants to use TPS2549-Q1 just like TPS2546-Q1.
This is because we want to minimize changes to the board and product specifications.
・Recommendation seems to be OPEN…
Part Number: TPS2549Q1EVM-729 Other Parts Discussed in Thread: TPS2549 I plan to use TPS2549Q1EVM-729 to build a demonstration prototype for up to 2.4A phone charging over a long (10-15 feet) cable. I plan to power the evaluation board with an external…
Part Number: TPS2549 Customer would like to evaluate dual USB port controller solution with cable compensation feature, but TPS2549 is a single port option. Could you please help check any suitable part for the cost benefit? Thank you.
Part Number: TPS2549-Q1 hi team,
My customer use the TPS2549-Q1 in a car infotainment project as a USB2.0 OTG port. as below. Find the TPS2549-Q1 can't blocking the reverse voltage.
When the system power down, and the external USB device(a laptop…