Part Number: TPS2556 Dears,
My customer needs IEC62368-1:2018(3rd) CB Certified Report.
Could you please provide it?
In the product folder I could find IEC62368-1:2014(2nd) version, however I could not find IEC62368-1:2018(3rd) version.
If it has not been…
Part Number: TPS2556 hi Teams:
According to the customer's feedback, the UL standard number of Ti seems to be wrong. It's best to provide the UL certificate?
Part Number: TPS2556 Hi team,
My customer has below questions about TPS2556 protection.
If Fault-pin is not used, should I float the pin or tied to ground?
Could you please introduce the recovery mechanism of two-level overcurrent protection and overtemperature…
Other Parts Discussed in Thread: TPS2556 Hi team,
I have questions on Equation 6 & 7 in tps2556 datasheet. Could you please double confirm whether the datasheet is right?
1. For equation 6, I think it should be:
2. For equation 6, I think it shouldn…
Part Number: TPS2556-Q1 Other Parts Discussed in Thread: TPS2556 Hi Team,
Please see the attachment. We may have another VBUS voltage on output side. If the VBUS voltage on output side is occur and then EN will be high to let TPS2556 turn off. (please…
Part Number: TPS2556 Hi, Team,
Customer found the over current response time in TPS2556 is longer than the topical values on datasheet. Could you help to check and give a comment? Thanks,
Oliver Ou
--------------
Figure 1 is a current-limit circuit using…
Part Number: TPS2561A Other Parts Discussed in Thread: TPS2549 , TPS2547 , TPS2556 , TPS2559 Tool/software: Hi,
I'm looking for a DCP support IC similar to TPS2561A but it should support 5V/3A power negotiation
Please suggest me a part
Hi Poorti,
Equation 1 in section 10.2.1.2.2 ( https://www.ti.com/lit/ds/symlink/tps2556.pdf ) approximates the resulting overcurrent threshold for a given external resistor value (RILIM).
With a 27.7 kOhm resistance, the Ios_min is around 3652 mA, which is…