Hi Prabhakar Lad,
Please can you help us to debug below gstreamer issue? (Logs attached below) input is 720*576 PAL from dvd player.
root@dm365-evm:~# gst-launch-0.10 TIDmaiVideoSrc videoStd=D1_PAL videoInput=comp osite ! fakesink gst-launch-0.10…
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: AM5718 , DRA722 , PMP Hi TI Team,
I am using TMDXIDK5718, REV 1.3B and ti-processor-sdk-linux-rt-am57xx-evm-06.02.00.81-Linux-x86-Install.
This is working fine and i can see complete log on…
Hi Eyal,
I have checked that ROOTFS path exist and is writable. Full Kernel log is as below. Attached log is too long. Please see it. Error is regarding wlan0 interface in kernel log is given.
-------ifconfig wlan0 up------
ifconfig: SIOCGIFFLAGS…
Hi Yan,
The link got accidentally deleted, please find a snapshot of the link that you are trying to access, we will have it restored shortly.
Regards
Karthik
/cfs-file/__key/communityserver-discussions-components-files/791/Processor-SDK-Linux…
Hi Hillman-san,
Thanks for your response.
As a confirmation, there is a function that can output TX_TCLK by Reg 0x00C6 [4] of DP83867. Is this correct?
According to the attached Tektronix document, Test mode 3 needs to be set in Step 2 of "Jitter…
Part Number: WL1835MOD
Hi, I want to follow-up on the issue I discussed a month ago. Here is the link for that. https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/993558/wl1835mod-wl1835mod-bluetooth-halted/3671061#3671061…
Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: AWR2243 I am using the "PROCESSOR_SDK_CASCADE_RADAR_03_08_00_00_prebuilt.exe" which is downloaded from :
https://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/latest/index_FDS…
Hello Amit. Thank you for your replay fast. I write new screen for attached file(Extern EEPROM: Onsemi EEPROM)
1. What is the use of Quick Command Here? => I just test Quick command code. The result is same without Quick command code. I will delete…
Part Number: TPS61170 Tool/software: Webench Our customer consider to use TPS61170.
They are checking gain/phase margin using with WEBENCH and excel spread sheet.
Vin=7.2V~8.8V
Vout=10V
Iout(Max)=400mA
When they check phase gain margin at…