Part Number: TPS2561A Other Parts Discussed in Thread: TUSB8042A I have a question about the circuit that supplies power from the output of TPS2561A to USB_VBUS.
When the output of TPS2561A is turned off, the electric charge accumulated in the output…
Part Number: TPS2561A Hi,
My customer would like to know if there is a single channel version of the TPS2561A?
They really like two features of the 2561A that make it attractive for their application. First the device has a soft current limit (i.e.…
Part Number: TPS2561A Other Parts Discussed in Thread: TPS2513A , TPS2513A-Q1 Hi there,
Below is our design requirement.
1. Four USB type C ports, providing maximum 5V/2A each port, no data transmission
2. Limiting total power output, 5V/4A, to keep system…
Part Number: TPS2561A-Q1 Other Parts Discussed in Thread: TPS25810-Q1 Hi Team,
Can you please advise with following request?
"
Do you have a power switch product with the same profiles as the TPS2561A-Q1, but with USB2.0 features as well as Type…
Part Number: TPS2560 Other Parts Discussed in Thread: TPS2561A , Tool/software: Hi team,
What is the difference between TPS2560DRCR and TPS2561ADRCR? Are they the P2P device?
What is the difference between DRC and ADRC?
BR,
Comi
Part Number: TPS2561A Hi,
I would like to know if the TPS2561ADRC has some backdrive protection.
If the OUT pins have a voltage apply on them but the IN is floating (0V) and EN pins is low @ 0V, will there be some backdrive current flowing from the OUT…
Part Number: TPS2561A Hello Guys,
Good day.
Just like to inquire if the ENx pins need Voltage to operate normal or can we leave the pins floating so TPS2561A operates as normal?
Thanks in advance!
Art
Part Number: TPS2561A Hi
Need urgent help from your compliance safety who do UL 60950 certification for IC TPS2561A.
We need to know if this IC is certified to IEC 60950-1 ANNEX C of IEC 60950-1 -2013 EDITION. IF so can you please provide us the CB certificate…