Part Number:
Hi, TI E2E teams
I have a project uses the chip of TPS25762.
i have finished PCBA. but i don't have base firmware package to download.
Would like send me the base firmware package to my email, tks.
Part Number: TPS25762-Q1 Other Parts Discussed in Thread: TPS25772-Q1 In application note <<TPS2576x/TPS2577x-Q1 Source Power Policy Management>>
we can manually set each port power delivery and the total power sharing between them, how could…
Part Number: TPS25762-Q1 Is it possible to obtain an output of 20V 3A using TPS25762-Q1 from 12V 5 A input through the USB out for powering up a device. If yes please provide the constraints and requirements for the above circuit setup.
Part Number: TPS25762-Q1 We are currently evaluating if the TPS25762-Q1 will work for our use case. I did come across questions I would like answered before we create a custom PCB. In the datasheet Figure 10-1 shows a configuration without any EEPROM…
Part Number: TPS25762-Q1 Hi,
Customer is looking for PD control integrated buck boost but no need AUTO grade, could you please recommend a function and spec similar solution to me? Thanks.
Part Number: TPS25762-Q1
Now we have a trouble, that is occurred new our designed board.
Problem is not able to download firmware to EEPROM.
It's 87% stop. We did it 2pcs boards. Result is same, both 87% stop.
What kind of factors for this error…
Part Number: TPS25762-Q1 Hi,
can you please share an internal register map and descriptions for the TPS25762-Q1? We want to access these registers over I2C2 from a system MCU and get the diagnostic data, similar to EVM. Is there some programming manual…
Part Number: TPS25762-Q1 Hello. I have developed a circuit that incorporates the TPS25762-Q1 for USB-C charging and a Realtek RTL8152B-VB-CG network adapter for use with an iPad. Schematic below. Before configuring the TPS25762-Q1, I was able to get the…
Part Number: TPS25762-Q1 Hi,
I have a customer who uses the chip of TPS25762, and would like to know whether the firmware supporting 65W can be provided?
If the customer applies on the official website simultaneously, can we speed up the processing?…
Part Number: TPS25762-Q1 Hi support team,
is the EEPROM absolutely necessary or can it be left out?
I thought that if you can load the firmware via USB-C or via I2C (MCU), you could omit the EEPROM?
Please give me a clear statement.
Thank you