Part Number: TMS320F28377D Hello,
I have a number of choices on how I can do data transfer between the LAN 9252 and the MCU.
1. Data/Address multiplexed memory interface (most preferred)
2. An indexed/non-multiplexed memory interface, address and…
What happens if I set the registers other than the instructions below?
1) Page 931 LCD_C Controller 35.3.5 LCDCVCTL Register NOTE: Settings for LCDREXT, R03EXT, LCDEXTBIAS, VLCDEXT, VLCDREFx, and LCD2B should be changed only while LCDON = 0.
2) Page…
Part Number: TUSB2036
Dear All,
My Japanese customer has a question about TUSB2036. The question is below:
I need to connect a low-speed USB device to a USB host that supports only full-speed. Is this possible by inserting TUSB2036 as a HUB between…
Part Number: TMS320F280049C Hi!
Please, I don't understand the definition of the GPIO41 - GPIO55.
In Table 4-1 page 27 (attached file tms320f280049c.pdf), there is a definition of this IO pins. But, this GPIO is not physical because they don't appear…
Hi Bin, I have kept the board with power on & off for 1000 times and out of which 20 times it failed because of this error along with some kernel panic. Do you use the root filesystem provided in the SDK? No i have been using customised rootfs just with…
Hi Anil,
Please take a look at the attached TRM (spruhm8g.pdf). You will find the answer in section 2.2.1 Device Identification. Let us know if you need further assistance.
Cheers!
Krishna
dual_core_delfino_spruhm8g.pdf
Part Number: BQ27426EVM-738 Dear Sir:
We use BQ27426EVM-738+BQ27000GDK for battery cycle learning,After the software is incorporated into the script, it can only be charged to 99% in the charging test, and the battery voltage is 3.4V lower than the…