Part Number: TPS25910 Dear Sirs!
I have a 14,5VDC power supply, I put the TSP25910 in series with it. I have some small load on the TPS25910's output and there is a big one: 14,5V/2,2A. I set the current limit to 3,5A
Unfortunately this load made…
Part Number: TPS25910 I am trying to understand the limits published in the datasheet for the ENABLE pins Threshold voltage ? I would like to model this input circuit using external components.
But need better understanding of the circuit. Yes a 10Meg…
Part Number: TPS25910 Dear SIR:
Good day!!
Would you help to review the circuit and have any recommend and advice for the circuit ?
Thanks PWR_TI_Review.pdf
Part Number: TPS25910 Other Parts Discussed in Thread: INA219 , TPS2595 , LM25066 Dear Team,
Originally the customer only using TPS25910 for current limit.
They wonder do we have current limit+current&voltage monitor device all in one.
Do you have any…
Part Number: TPS25910 Other Parts Discussed in Thread: TPS25940-Q1 , TPS2595 , TPS24750 , TPS25982 Dear Sir/Ms.
The customer's purchaser request RD is looking for 2nd source to SY6875A. Before we have recommended TPS25910 and TS25940-Q1 but the specifications…
Part Number: TPS25910 Other Parts Discussed in Thread: TPS2590 To avoid the start up current limit, im using a Mosfet after the output of the TPS2590 to switch on loads. When using a electronic load in constant resistance mode, this works fine. I can switch…
Part Number: TPS25910 Hi there,
My customer is looking for an eFuse solution where Vin(max) is 19V and the continuous output current required is 10 A.
My customer prefers solution with integrated MOSFET so our HotSwap solution does not fit here.
I'm curios…