Part Number: TPS2592AA Other Parts Discussed in Thread: TPS25924 Why is TPS2592AA status changed to NRND (not recommended for new designs) and what is the replacement for it.
Part Number: TPS2592AA Other Parts Discussed in Thread: TPS25981
Hi Team,
Customer followed old design with TPS2592AA. Vin is 12V. current limit is 2A.
Customer need to support effuse output pin short to ground function in new platform.
However, customer…
Part Number: TPS2592AA Hello Team,
My Customer is using the TPS2592AA and noticed the change in the datasheet of Rilim from 150K to 100K. They wanted to know what the issue was that caused the reduction in the range of this setting? They are aware that…
Part Number: TPS2592AA Other Parts Discussed in Thread: TPS25924 Hi Sir / Madam,
The following part no: TPS2592AADRC is mentioned as NRND in your website.
Actually, all our old designs contains the TPS2592AA IC, which are in the production stage write now…
Hi,
I apologize that no one has followed up with your question. I'm going to close this thread, but if you still have a question please feel free to post a brand new thread instead of replying to this one. We will do our very best to respond within…
Other Parts Discussed in Thread: TPS2592AA , TPS2592AL , TPS2592BA , TPS2592BL , TPS2592ZA Hi,
Because TPS2592AA is NRND, and my customer would replace it by TPS259240.
Please help to recognize the difference between TPS2592AA and TPS259240.
I know the Current…
Other Parts Discussed in Thread: TPS2592AA Dear Sirs
My customer use TPS2592AA for their +12V protection.
When power up, the load will over 3.7A in 200ms. (peak current over 3.7A)
And TPS2592AA will work to protect the output circuit.
If they do not want T…
Other Parts Discussed in Thread: TPS2592AA Dear Sirs
Please help review the following circuit about TPS2592AA.
I want set UV is 5V.
1.Is the R1 and R2 value right?
2.Is the pin BFET floating ok?
3.Is there any comment about the circuit?
Thanks
BRS
N…
Other Parts Discussed in Thread: TPS2592AA Hi,
Our customer plan to use TPS2592AA to prevent inrush current and over voltage at hot-plugging event. Then they're concerning damage for TPS2592AA if VIN is connected first before GND. Please refer attached…