Thanks Dinesh,
However I am looking to use the TPS2592 ZA part since I need to operate at 12V and limit at 1A. The TPS2592AA part data sheet, that Figure 31 refers to, is 2A - 3.7A.
The same 'Accuracy vs Overload Current Limit' graph does not appear…
Hi Luiz,
Thanks for sharing the information.
Good ... Now with TPS2592AA you can go up to 3.7A .. and if you still need more current with TPS2592AA , I can help you to use two devices in parallel to drive 7.4A load.
Please let me know for the further…
Other Parts Discussed in Thread: TPS2592AA Hi,
Intend to use TPS2592AA for Safe Startup of Brushless DC Fan (reference App Note attached) .The reference design shown is for a Fan with higher current requirement.How to I simulate to find out component values…
Hello Berry ,
22uF Cout is fine.
Assuming your Input voltage is 12V, We do not recommend the ILIM resistor (R116) value to be more than 100k for the TPS2592AA, when your ambient temperature is within 0°C to +85°C. and if ambient is –40°C to +85°C …
Hi Juan,
For new designs, recommended pin to pin, drop-in replacement for TPS2592BA is TPS259231.
The new device can support load current in the range of 1A to 5A and meets your requirement of fast trip comparator characteristic. Fast trip comparator…
Other Parts Discussed in Thread: TPS2592AA Hello,
Regarding the TPS2592AA device: The Evaluation module user’s guide has D5 in the schematic connected to BFET & OUT pins. This is not shown in the datasheet examples.
Could you please explain what…