Other Parts Discussed in Thread: TPS2592AL Hi,
I have a question about TPS2592AL.
What is the mosfet gate voltage during the overcurrent protection?
Is this devices have a leakage current from the gatecontrol to the output?
Regards.
Kenta Watanabe.
Other Parts Discussed in Thread: TPS2592AL Hi,
I have a system design with TPS2592AL. Currently, I have a issue when the power up.
The Condition are
Vin= 12V, UVP setting =9V, Rlim=143K, dv/dv= floating, BFET=floating,
Cout is ~220uF
Usually, I can get…
Hi,
We would like to ask about Thermal Shutdown function.
Where is a sensing point of junction temperature(Tj) of device?
I believe that Tj is sensed at Power PAD.
Is my understanding correct?
[Datasheet page.14]
The device also has built-in thermal…
Other Parts Discussed in Thread: TPS2592AL Hi, Would you mind if we ask TPS2592ZL and TPS2592AL? <Question> Fault response of TPS2592ZL and TPS2592AL are latch-off. When the UV failure occurred, which will the fault response be Auto-Retry or Latch-off? …
Hi,
We would like to ask about power dissipation during start up.
I believe that the Limits at CdV/dT = 27nF should be "OK" in following table.
Is my understanding correct?
Regards,
Kanemaru
Other Parts Discussed in Thread: TPS2592AA , TPS2592AL , TPS2592BA , TPS2592BL , TPS2592ZA Hi,
Because TPS2592AA is NRND, and my customer would replace it by TPS259240.
Please help to recognize the difference between TPS2592AA and TPS259240.
I know the Current…
Hi Juan,
For new designs, recommended pin to pin, drop-in replacement for TPS2592BA is TPS259231.
The new device can support load current in the range of 1A to 5A and meets your requirement of fast trip comparator characteristic. Fast trip comparator…