Part Number: TPS25948 Other Parts Discussed in Thread: TPS2663 Hi team,
When I searched for an efuse that met the required specifications on TI.com, I found something like the image below. So I have a question: Can the product shown below with Vin (max…
Part Number: TPS25948 Hi Team,
I would like to know about Ball material of TPS259480LYWPR (DSBGA).
<Question>
If the lead isn’t plated, please tell me the lead material.
If the lead is plated, please tell me the plating material.
(For example…
Part Number: TPS25948 Other Parts Discussed in Thread: TPS25947 Hello,
My customer is looking for a hot swap controller with the conditions below.
- Typ 12V, Max 3A
- Current limit and Reverse current protection
- A function that can provide output…
Part Number: TPS25948
Dear TI E2E Support,
Noticed that in the TPS259 48 datasheet the orderable info is registered as TPS259 84. Whom can we contact for this issue?
https://www.ti.com/lit/ds/symlink/tps25948.pdf?ts=1692610112590&ref_url=https%253A%252F…
Part Number: TPS25948 Hi,
Does TI have below E-fuse protection IC with AEC-Q100? I found some prodcut can meet below spec but seems no one have AEC-Q100.
Vin 9V~18V
Iout 8A
Thanks!
Jeff
Part Number: TPS25948 Other Parts Discussed in Thread: TPS2597 , TPS25947 Hi team,
Typical application shows Cout is 47uF.
But for Circuit Breaker eFuse, such as TPS25947 and TPS2597, Cout is 470uF at typical application.
Is it common comparison between…
Part Number: TPS25948 Other Parts Discussed in Thread: TPS25981 Hi team,
Look like our eFuse are all just limiting current to certain current limit value (often set as ILIMIT pin resistor) when overcurrent event happens. Is there any IC being able to shutdown…