Other Parts Discussed in Thread: TPS25948 Hi, TI expert
A customer is inquiring about alternative options for the FPF2895CUCX (ON Semiconductor), which is currently under review as a Current Limit Switch.
- Application : 5G PDA cradle
FPF2895C-D.PDF
Is…
Other Parts Discussed in Thread: TPS25948 Hi,
I am Elaine, DFX Engineer from Plexus Corp. I am working on package model build for MPN TPS259480AYWP.
Noticed that there is no body and pins dimension for MPN TPS259480AYWP in the datasheet.
Please help to…
Hi Tiger,
Thank you for the clarification. Since I am working with 2 power inputs (USB Type-C and DC Barrel), I searched for Priority Power MUXing and found several options like TPS25983, TPS25948 and TPS25947. However, I could not find any helpful reference…
Part Number: LM7310 Other Parts Discussed in Thread: TPS25947 , TPS25948 LM7310 support team
The LM7310 datasheet is not mentioned on UL2367 and IEC62368. Has LM7310 already gotten them as same as TPS25947 and TPS25948?
If YES, please share CB report #…
Part Number: TPS66120 Other Parts Discussed in Thread: TPS25948 Hi team, my customer need a USB type C PD power switch and the current limit is about 7A. However, I only see TPS66120 on the website, which current limit is 5A. Are there any other products…
Other Parts Discussed in Thread: TPS25948 Hi Team,
my customer is searching for load switch device with OVP/OCP used in smartphone.
Vin= 3-5.5V, Vin max = 28V, Iout=2A, Ron max = 120mohm, reverse block.
ESD: IEC61000-4-2, air discharge >=12KV, contact discharge…