Part Number: TPS2595EVM Tool/software: Good evening TI,
I'm stuck with a noise problem with the TPS2595EVM (TPS259541, U3) and would appreciate any help!
Situation:
My team wants to build a cable that prevents short circuits at the output port …
Part Number: TPS2595EVM As for input voltage for V EN of TPS259541DSGR, the datasheet says as below;
"For supply voltages greater than 6V, it is recommended to use an appropriate resistor divider
between IN, EN and GND to ensure the voltage at the…
Part Number: TPS2595EVM Have 12V being supplied at VIN from a power supply. J1 and J3 are open. No matter what ILIM setting I choose or whether there is a load or not VOUT1 is constantly at 3.8V and VOUT2 is constantly at about 5.8V, so it seems they…
Part Number: TPS2595EVM Hi support team,
In the original question, Cout is recommended to be 1μF for decoupling purposes. This EVM is also equipped with 22μF or 100μF. What is the purpose of increasing Cout?
Regards, Dice-K
Part Number: TPS2595EVM Other Parts Discussed in Thread: TPS2595 Hello team,
We’re looking at using TPS259530 for their design. They tested the eval board and it all looks reasonable except I get one result I don’t expect. If the device is started into…
Part Number: TPS2595EVM Other Parts Discussed in Thread: TPS2595 Hello
Customer connect to DUT and test 19Vin. The waveform looks abnormal as below. Does the chip enter thermal cycle protection or any others root cause? Thank you.
BR
Patrick…
Part Number: TPS2595EVM Thanks for getting the TPS2595EVM to us on quick turn.
I am using VOUT1 (TPS259520) for the following experiment.
My input is from a bench power supply - 3.3V, current limit set to 5.0A.
I am setting the current limit…
Part Number: TPS2595 Tool/software: Hello team,
My customer is evaluating TPS259541 with TPS2595EVM.
When testing current limit function, FLT looks auto-retrying, even if Vout is still 0V.
Is this expected? Can you explain why this periodic waveform…
Part Number: TPS2595 Hello,
My customer has a question about the TPS259541 design.
Could you please tell us the reson why SMBJ16A-13-F TVS was selected for the TPS2595EVM input stage?
The max clamping voltage of the SMBJ16A is 26V. But, the absolute…