Part Number: TPS2596 Hello I'd like to limit the current from IN to OUT with 0.3A limit, but also i wanna power my circuit using OUT to IN path. I possible to do that ? or is suggested to put a schottky diode from OUT to IN in order to avoid current…
Part Number: TPS2596
Hello team,
Can I use TPS2596 like a high side switch on the diagram below? The app note: Driving PWM Loads with TI High-Side Switches says high side switch can be used as high side protection for PWM generator (Low side Driver).
…
Part Number: TPS2596 Hello,
I plan to use TPS259620DDA in my design. The data sheet states that in order to select 5.7V overvoltage clamp I need to connect OVCSEL pin of the device to GND via 400K resistor. However, 400K is not a standard value. The standard…
Part Number: TPS2596 Hello,
I plan to use multiple TPS259620DDA devices in my design. These are latching parts, and my understanding is that to unlatch I need to cycle the Enable pin. So, I have 2 questions.
1. What is the minimum time to drive the Enable…
Part Number: TPS2596
Hello,
I've 15V as main supply and a 12V lead acid battery to backup it.
I need a voltage limiter circuit to drive a 9~12 siren, and protect from short circuit.
TPS259621 clamp output voltage at 13.8V, using 2x diode I think…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS2597 Hi, If my understanding of this part is correct, the shutdown of the device in short circuit failure relies on the Junction temperature exceeding the thermal shutdown temperature? This means it…
Part Number: TPS2596 Hello, I intent to use TPS259630 to a power management equipment, responsible to supply some sensors and drivers using cables from 5 to 15 meters.
I add reverse voltage protection, and a bead on input.
I'd like to know if it is…
Part Number: TPS2596
I was playing with this eFuse with an undervoltage clamp of about 2.41V and a 10.1V overvoltage clamp, I was also fusing for about .4 A using a 2k resistor as Ilm. I would like to run this system at a typical 8V but when the 8V passed…
I think the 2-3V is with 10's of amps of current but still I understand that even at more reasonable currents it is not down to 0.3V which is the max negative voltage supported by the TPS2596. Perhaps those Schottky diodes will help as you recommend.…
Part Number: TPS2596 Hi,
We have TPS259631 in our design.
We are trying to create and test the fault condition 'ILM Pin Short to GND' as shown in Table 3 of TPS2596 data sheet. But we are not seeing the FLT# signal getting asserted when shorting…