Part Number: TPS259827LEVM Dear all,
During startup, is there a graph showing the relationship between the input voltage or input current of the TPS259827L and Ron?
Because we found that the ON-Resistance calculated from the voltage difference and…
Part Number: TPS259827LEVM Hello Respected This is Thilaga from Flex We are currently working with one of our manufacturing plants to collect below information Site: Zhuhai Please provide us the MSL data for the below part
MPN;
MPN
MFG_NAME…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS1689 , TPS1685 Hi, I have a hard time making the TPS259827LNRGET work.
I am testing it with an electronic load.
It power up fine
I can start the Electronic load at 500mA
Then if…
Part Number: TPS259827LEVM Tool/software: hello
the datasheet shows a default design with a cout of 220uF . do i need to have 220uF capacitor next to the part additional to my CL or that is just a example and the part itself doesn't need any COUT .
Part Number: TPS259827LEVM Hello, I am using TPS259827 in a design. Here are the application details: VIn=12V Ilimit=12A delay-before-circuit-break =100uS Retry-time-after-fail=4.7S
I tested the circuit break behaviour with an Electronic Load and above…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS25983 , TPS25982 Tool/software: Hello,
I am looking into implementing the TPS259827LNRGER device into our current system as we are facing difficulties with our current eFUSE internal reverse…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: LM5066 Hello,
I would like to ask about the chip in the title. I use this chip as an e-fuse on my 24V power line, but I cannot get anything on the output, it is 0,45V and I am wondering wether…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS25983 , TPS25982 Tool/software: My previous question :
TPS259827LEVM: TPS259827ONRGET E-fuse Output remains ON when EN/UVLO is at 0V"
This still occurs regularly and I'm still unclear…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: TPS25982 Tool/software: Such as Figure1. When the Vin voltage is stable, if you turn on the Enable pin at this time, you will see that the Vout voltage slowly rising. What will happen in this…
Part Number: TPS259827LEVM
Hi team,
In this EVM, PG pin is pulled up to 3.3V when J7 is connected 2-3.
But in User's Guide figure3 seems Vpg is around 2V in asserted. Why this voltage drop happen?
teritama