Part Number: TPS2660 Tool/software:
According to tips, some questions need your clarification.
1. Can we choose 100V to use if diode blocking voltage of my current case is 80V? It's better, right? Or it's not critical and jsut make sure higher than Vin…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS22998 Tool/software: Hi Team,
TPS26601 as load switch.
Vin/Vout=48V
Iout/Ilimit=0.7A
I_fastrip= 1A
What is the Cout capacitance to be used in design?
Regards,
Vidhya
Part Number: TPS2660 Tool/software: I tried simulating TPS26601 Transient Model in Start Up state. I see difference in behavior of simulation output vs calculated results.
Calculated Values of R1,R2, & R3 for OVP & UVLO fault as per TI Spreadsheet calculator…
Part Number: TPS2660 Tool/software: Hi Team,
The TPS2660x and TPS2663x series provide the certificates for fire protection purposes according to IEC-62368-1/2.
Do they also offer the certificate for the latest -3 (IEC-62368-3 Version 2021)? If not, is…
Part Number: TPS2660 Tool/software: My design currently has the FLT pin tied to IN though a red LED and a 10K resistor. In normal use, this gives a suitable visual indication for under voltage, over voltage, and over current situations.
However, am looking…
Part Number: TPS2660
Hi. I have a some question about TPS26601 load current detection. What is the minimum detection current? Does the IMON signal have an offset value for current detection? I would like to detect a load current of 100mA. Is this possible…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS1653 Tool/software: Hi
The TPS26601 is designed with /SHDN, device shutdown at logic low.
We are searching for the part like TPS26601 but shutdown @ logic high, we also need the output discharge…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS2663 , Hi
Could you help introduce suitable products. This is a dual power input design, the specifications are as follows,
Dual input, one out,power load switch
Power reverse solution
Overload current…