Part Number: TPS2660 Tool/software: Under-Voltage Lock-Out function is not needed, the UVLO terminal must be connected to the IN terminal as per datasheet recommendation.
Similarly if OVP is not required should the pin connected to IN?
Part Number: TPS2660 Other Parts Discussed in Thread: TPS2662 , Is the TPS2660x tolerant to negative voltage transients on the output? As would be seen when opening the e-fuse with an inductive load on the output.
Thank you and best regards
Part Number: TPS2660 Other Parts Discussed in Thread: TPS1663 Hi BU friend,
Here is a requirement from customer of Efuse:
1.The input of the device is a 12S battery, with a maximum voltage of 50.4V and a minimum voltage of 26V; the maximum operating…
Part Number: TPS2660 Application node: slvaek7 is described about failure mode for TPS2660 below.
Please let me know about meaning of failure mode;
・"OUT stack on" is equal to input ~ output short, is it correct?
・Are there any trends regarding…
Part Number: TPS2660 Please give me some suggestions for Efuse application (48VIN).
1. TVS selection for input side
a. Reverse voltage
b. Breakdown voltage
c. Clamp voltage
2. Schottky for output side side
a. Reverse voltage
b. Surge current
c. Forward…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS2662 Customer is doing the STO circuit with TPS26600PWPR for Robotics application. Few questions are here.
- Is enable function able to be implemented on UVLO pin of TPS2662?
Below is test on bench…
Part Number: TPS2660 I guess the equation of 11 is typo. it should be UVLOF(Falluing), not UVLOR(Rising). Could you help to double check on this! Very thanks.
Part Number: TPS2660 Dear Specialists,
My customer is considering TPS26602 and has a question about via size.
I would be grateful if you could advise.?
---
Datasheet P.49 EXAMPLE BOARD LAYOUT describes that Φ0.2 vias should be installed.
Are these…
Part Number: TPS2660 Hi,
We have some conversations with engineers and I think that eFuse TPS26602 PWPR might be influenced negatively by Bulk current injection tests of the DO160. I think that there should be a minimum of LC filtering before the eFuse to…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS2640 , 1. During a surge test, EFUSE was damaged when -3kV was applied to line to line or when -4kV from N to PE is applied, Efuse is damaged.
Waveform explanation below) CH1 is the EFuse input voltage…