Part Number: TPS2660 I guess the equation of 11 is typo. it should be UVLOF(Falluing), not UVLOR(Rising). Could you help to double check on this! Very thanks.
Part Number: TPS2660 Dear Specialists,
My customer is considering TPS26602 and has a question about via size.
I would be grateful if you could advise.?
---
Datasheet P.49 EXAMPLE BOARD LAYOUT describes that Φ0.2 vias should be installed.
Are these…
Part Number: TPS2660 Hi,
We have some conversations with engineers and I think that eFuse TPS26602 PWPR might be influenced negatively by Bulk current injection tests of the DO160. I think that there should be a minimum of LC filtering before the eFuse to…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS2640 , 1. During a surge test, EFUSE was damaged when -3kV was applied to line to line or when -4kV from N to PE is applied, Efuse is damaged.
Waveform explanation below) CH1 is the EFuse input voltage…
Part Number: TPS2660 Other Parts Discussed in Thread: TPS1663 , TPS2663 HI Team,
for safety regulations reasons customer needs to reliably limit the current.
They are already using TPS2660 for another project but now need a solution with a max current limit…
Part Number: TPS2660 I have reviewed both the datasheet for the TPS26600 and the App Report SLVA934A on how to handle the FLTn and IMON outputs during input reverse polarity. But I don't think things are clear concerning the final note on the SLVA934A…
Part Number: TPS2660 Hi TI team.
The board I am designing requires as one of its functions conduct power from a battery charger to a Li-Ion battery 10s (42 V max) and/or 13s (54.6 V max) charging at 2A.
I required the following protections:
* Transient…
Part Number: TPS2660 Hi,
From the datasheet for the TPS2660x, I see that there is there is pin (dVdt) that can be used to set the output voltage slew rate for in-rush current control.
Does this essentially fulfill the role of a load switch? If not, would…
Part Number: TPS2660 Hi Team,
About e-fuse TPS26600RHFR Since the example in the datasheet is double layer, Currently I have a new project is 8-layer layout.
need help in confirming the layout of the RTN plane. Currently, I plan L1, L2, L7, and L8 to be…