Part Number: TPS281C30 HI, I need to assess the voltage on the ILIM pin, to find the correct power rating of the RILIM.
We use an input voltage of 24V, KCL is 50A*kOhm, the current limit is 1A and the RILIM is 50KOhm (KCL/IOUT).
The datasheet in page…
Part Number: TPS281C30 Tool/software: Clarification on NC Pin (Pin 8) Connection for TPS281C30
I am currently working with the TPS281C30 and noticed a discrepancy between the datasheet and the evaluation board (EVM). In the datasheet, it is mentioned…
Part Number: TPS281C30 Tool/software: Need Spice model for simulation purposes. Could not be able to find simulation models in the library. Kindly provide us with the Spice model for testing purpose. Thank you.
Part Number: TPS281C30 Tool/software: Dear team,
TPS281C30 has NC pins 7,8,9. Can those be connected to GND for better thermal connection to the PCB or should they be not connected?
many thanks
Lutz
Part Number: TPS281C30 Tool/software: Hi Team,
Please clarify whether the part number TPS281C30B internal FET supports continuous current rating of 10A. Current limit mentioned as 10A but the electrical characteristics show continuous current of 6A…
Part Number: TPS281C30 Tool/software: Hi Team,
I am using the TPS281C30CRGWR,
With regards to the SNS pin, is it possible to connect this pin directly to ADC? i saw that there is no mention for it in the DS and that in some places we are putting…
Part Number: TPS281C30 Other Parts Discussed in Thread: TPS2H000-Q1 Tool/software: Hi there, I'm driving an inductive load with 24V PWM signals with 150HZ. The range of load current that is important to us is between 200-800mA. What is the most accurate…
Part Number: TPS281C30 Tool/software: Dear Sir,
I am wondering of there are any limitations to control the EN pin of TPS281C30 by a PWM signal in order to control the voltage output of the High side switch ?
Regards
Part Number: TPS281C30
Hello,
I plan to use the 'B' version of the TPS281C30 in a new design. I would like to dimension the current limit in such way that 2.75A will never trip the over current limit and to limit the max ICL as much as possible. …
Part Number: TPS281C30 What are all the differences between TPS281C30A and TPS281C30B? Tradeoffs?
Any cost differences?
How is the difference in current limit adjusted between the devices ie. what makes this difference?