Part Number: TPS3307-18M Other Parts Discussed in Thread: TPS3307 , TPS386000-Q1 Hi E2E,
Good day!
Do we have information regarding below inquiries?
1) does the TPS3307 have glitch immunity? 2) what is the minimum time MR has to be held low for the RST…
Part Number: TPS3307 Other Parts Discussed in Thread: TPS3779 , TPS386040 , Hi,
do you recommend the TPS3307-33DR for a new industrial design or is there an alternative that is similar and newer?
Thanks
Fred
Other Parts Discussed in Thread: TPS3307 I have a question about TPS3307-33.
Output of Reset signal is 3.3V.
But we want to sense 5V.
Can we use dividing resistance when voltage of VCC and SENSE pin is 5V?
Please check the attached document.
Best regards…
Part Number: TPS3307 Hi, I am using this part but there is a problem:
When MR pin is open, sometimes the part reset it self by accident. If this pin is not used, is it ok with connecting to VDD and using a 10nF cap for the filter to keep the noise from…
Part Number: TPS3307 Hi,
Can you drive Manual Reset (MR*) pin using open drain/collector IC output.
The block diagram suggest it has internal 14k ohm pull-up. Is this a internal resistor?
Best regards, Dhaivat
Part Number: TPS3307-18 Hi, all.
Td of tps3307 is prescribed with Min140~Max280 ms by the 25 degree.
How many is Td when using the full temperature range?
Do you have a temperature dependency chart of Td?
Best Regards,
Kobayashi
Other Parts Discussed in Thread: TPS3307 Hello.
My customer is currently in using TPS3307,now.
I have gotten a request about this product .
So, please answer me about TPS3307.
<Request>
The past made this such exchange.
e2e.ti.com/.../539211
Sorry, I have…
Hello.
My customer is currently in using TPS3307-33,now.
I have gotten a question about this product .
So, please teach me about TPS3307-33.
<Question>
The "VIT+" exists in the data sheet on page 2.
Does this voltage mean of "VIT- + Vhys" ?…
Product End of Life details required for new design
1.SN74AVCH2T45DCUR
2.TPS2051BDBVR
3.SN74HC365PWR
4.SN74AVC1T45DCKR
5.TXB0108PWR
6.SN74LVC1G08DCKR
7.MAX3223EIPWR
8.TPS542941RSAT
9.TPS51200DRCR
10.TPS3307-18DGNR
11.SN74LVC16T245DGGR
12.TPS386596L33…