Part Number: TPS3435-Q1 Tool/software: i want to use this IC in one of our product, for that we want to do circuit simulation.
can you please share the simulation module for Pin Configuration Option C DDF Package option.
for the below highlighted part…
Part Number: TPS3435 Tool/software: Hello TI Team,
I need to insert a watchdog Timer in my circuit and I have selected TPS3435AFACADDFRQ1 with the aim of respecting the following timing parameters:
Startup delay: 10 seconds
Watchdog Timer (twd) : about 10…
Part Number: TPS3435 Tool/software: Hello!
Can you please help me with more information for the following watchdog chip: TPS3435JFMAFDSER.
I see that this chip has a preset delay of 50s, but I want to scale it and I saw that the scaling could be 1, 2…
Part Number: TPS3435-Q1 Other Parts Discussed in Thread: AM620-Q1
Tool/software:
Hi Team,
I have a customer using
TPS3435CKHBDDDFRQ1
I could not find this OPN while searching. Can you please confirm this is a valid OPN.
Customer is using pushpull output…
Part Number: TPS3435 Other Parts Discussed in Thread: TPS3436-Q1 , , TPS3436 Tool/software: Hi team,
I noticed that the differences between TPS3435 and TPS3436-Q1 are below:
3436-Q1
3435
May I know what's "open window to close window ratio" and…
Part Number: TPS3435 Tool/software: Hi, TI expert.
A customer has requested a Watch Dog IC recommendation.
1. Input voltage 5V 2. After booting, if there is no signal (GPIO HIGH or LOW) from the MCU for a certain period of time (approximately 0.1s to…
Part Number: TPS3435-Q1 Hey,
I would like to use this chip (TPS3435-Q1) with a latched output functionality, but it seems it is not available. Is it possible to order that option?
Thank you in advance.
Zsolt
Part Number: TPS3435-Q1 Other Parts Discussed in Thread: TPS3430 , TPS3435 Tool/software: Hi TI,
I've been developing a system to be latched using an external open drain buffer based on the application note: snva837.
In this document, the implementation…
Part Number: TPS3435-Q1 Other Parts Discussed in Thread: TPS36 , TPS3436 , TPS35 , TPS3435 Tool/software: Hi TI,
I'm working on a project using the TPS3435AFACADDFRQ1.
Now we use this watchdog timer as a failsafe circuit to make sure the system is safe…